Other Parts Discussed in Thread: TPS65982, HD3SS460, HD3SS3212
Hi team,
I have a few questions about alternate mode impementation of TPS65982.
First, how does the integrated HS MUX work? According to the datasheet, the relevant signals include USB 2.0 and SBU, does this mean the two signals couldn’t work at the same time? If so, USB 2.0 signals are disabled if system is in an alternate DP mode, right?
Second, about the external SS MUX, since TPS65982 already has HS MUX inside, HD3SS460 is not applicable any more in this system, right? (since HD3SS460 also has low speed mux inside)
Third, also I didn’t see any MUX like HD3SS3212 or HD3SS460 in TPS65982 EVM, only the switch bank S1, so how can the system perform signal routing in alternate mode specifically?