Other Parts Discussed in Thread: TUSB211
Hello,
We have a Notebook project and using TUSB211. The PCB trace distance between host controller and the USB port is 12000mils. Can TUSB211 support such distance?
thanks.
Mingmo
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: TUSB211
Hello,
We have a Notebook project and using TUSB211. The PCB trace distance between host controller and the USB port is 12000mils. Can TUSB211 support such distance?
thanks.
Mingmo
Hello,
The TUSB211 should be able to handle the distance, however I recommend to include two re-drivers on the signal path (one close to the Host and the other close to the connector) and as a first approach populate only the TUSB211 on the connector side.
Regards,
Diego.