This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Will TI have also a Stand-Alone USB 3.0 Controller?



Will TI have also a Stand-Alone USB 3.0 Controller? I develop an Industrial PanelPC using a High-Performance ARM based Microcontroller and like to add a USB 3.0 port. When will TI develop a 2000MHz (or more) Ferari? The OMAP 3530 is very nice, but could have 3 times the speed to kick off this NDA nightmare of Marvel. Thanks Michelle