Hello,
I wanted to know if the TPS65982 family of devices could support the MHL protocol over alternate mode or if additional firmware would be required? If it doesn't currently support it are there plans to support it?
Thanks,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
I wanted to know if the TPS65982 family of devices could support the MHL protocol over alternate mode or if additional firmware would be required? If it doesn't currently support it are there plans to support it?
Thanks,
Michael,
I definitely need to elaborate on this point to be more clear.
There are 3 approved Alternate Modes that support Video, but DisplayPort is the most widely implemented Alternate mode that explicitly supports Video and USB3.1 data simultaneously and is geared towards a Type-C to Type-C port ecosystem where the cable is universal but the Video data follows the standard DisplayPort specification. The DisplayPort for USB Type-C standard also has a fully implemented PD compliance test that is certified at USB-IF workshops.
These are the 3 approved Alternate Modes capable of video and some distinctions:
Although the MHL specification does include the ability to transmit USB2/3 data and appears to have similar capabilities, but the market trends have shown that DisplayPort has been adopted by most industry leaders. In addition, the landing page for MHL over USB Type-C also has an FAQ section which says that MHL is working with the USB-IF and will have full compliance testing [at a later date] ()
Because the TPS65982 is a FW-based part and the PD Policy Engine is flexible/configurable, we still have the ability to implement the MHL specification in end equipments that require it.
This can be done quite easily when the TPS65982 FW is configured with a "User-Defined Alternate Mode" that transmits the MHL Specific-Vendor ID (SVID), the Mode #, and Payload data (VDOs) required to Enter the Alt. Mode automatically.
To send any Vendor-Defined Messages that are unique to the MHL Alt. Mode, an embedded controller (EC, or I2C Master) that controls the TPS65982 can be used to build simple messages and send VDMs ('VDMs' ASCII command) for configuration and attention PD messages.
If the customer decides to implement ThunderBolt and/or DisplayPort, it is already taken care of automatically in the standard FW.
If the customer still wishes to implement the MHL Alt. Mode, we have a framework set up to get moving quickly and start testing a system. If this is the case, please follow-up and we can explain the "User-Defined Alternate Mode" features in more detail.