This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TUSB4041I GANGED configuration

Guru 16770 points

Other Parts Discussed in Thread: TUSB4041I

Hi

We have question of TUSB4041I GANGED setting.

TUSB4041I supports Ganged operation using enable bit at PIN 10 (GANGED/SMBA2/HS_UP).

According to the datasheet, PIN10 has internal pull down and ganged mode is disabled by default.

However, TUSB4041 EVM user guide (SLLU227) shows following description at page 5 SW2_2 (on) definition.

>The TUSB4041 has an internal pullup on this terminal, so ganged mode is enabled by default.

What is the default state of PIN10 of TUSB4041I?

If PIN10 is not connected, which mode is set?

Bestregards