I have been trying unsuccessfully to use the 2.9 TPS65983 tool to customize the Apex Creek 2.9 project. While I am able to create a binary from the Apex Creek 2.9 project, it does not work with the AR. I reported this to Intel and they sent me an updated Apex Creek project, but the 2.9 TPS65983 tool gets and exception when trying to write the binary file, so no file is created.
The lack of a working 2.9 TPS65983 tool and Apex Creek project has stopped the TB3 certification of my SEL and SE-I AR based products.
Is there an updated TPS65983 tool and Apex Creek project available that I can use and if not, when can an update be made available. T