Other Parts Discussed in Thread: SN65LVP20
I would like to use the SN65LVP20 device in a new design.
A couple of quick questions on input termination for the SN65LVP20:
1) Does the SN65LVP20 have internal termination on its inputs or is external termination required?
The .pdf does not state & there are not any examples.
2) If the SN65LVP20 has internal termination, is this common to other "LVP" devices (ex. CDCLVP1210, CDCLVP1024).
I need to use all 3 devices and want to make sure the termination is correct as I am ready to move forward to layout.
Also, any examples that show input / output termination would be helpful.
Thanks in advance,
- Michael Lawson