Other Parts Discussed in Thread: DS125DF111
We would like to know the values of the DFE taps in an absolute sense, as a function of the DFE tap register settings. For example, for the DS125DF111, tap 1 has a five-bit field and taps 2-5 have a four-bit field, along with a polarity bit for each tap. What is the actual value of the DFE tap as a function of these quantities, if the main (cursor) tap is normalized to +1 when presented to the DFE summing node? Is the range of each tap from -1 to +1, and tap 1 simply offers higher precision than the others, or do they have different ranges? Thanks.