This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS25810EVM query



Hi,

Looking for integration test set up diagram (connection) for TPS65982EVM to use in UFP configuration as the schematic is some what complicated to understand where to connect the load and power for different configuration.

  • Do you already have the TPS65982EVM on hand or just the TPS25810EVM? The TPS25810EVM can be used stand alone using the Rd and Ra on board jumpers to simulate the UFP. Loading can be applied at J7.

    But, using the TPS65982EVM as the UFP is also fairly simple. Right out of the box, you can simply connect TPS25810EVM to TPS65982EVM with the type C cable. Use the S1 dip switch bank to select a UFP configuration and follow the directions in section 5.3.3 of the EVM user guide. You can use the VBUS and GND test points to apply the loading on the UFP end.