This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TCA9555 SDA, SCL and INT pins

Other Parts Discussed in Thread: TCA9555

I have a customer that wants to use pull-up voltages above Vcc on the SDA, SCL and INT pins only. These pins are not really described in detail. I am assuming that these pins do not have pull-ups, but I am not 100% certain. Can you verify if using a pull-up voltage above Vcc (Vcc=2.5V; Vpullup=3.3V) on the SDA, SCL and INT will cause an issue? Can this damage the part in any way?

From what I have read in the forums it appears that the Icc of the TCA9555 might increase in this situation. Is this true? Can you verify the increase that they might see and why?

Can you send me a picture of these inputs showing the FETs etc.?

Thanks for your help with this!

Richard Elmquist