Other Parts Discussed in Thread: SN75DP159
Hi,
On a number of products we are using the SN75DP159 as a HDMI Tx retimer.
When running HDMI 2.0 compliance test all products fail the intra-pair skew (P vs. N) compliance part with approximate the same value.
Measured skew is approximate 30-40 ps while the requirement states about 24 ps (0.15 * Tbit).
All other compliance test passes with good margin.
Our layout is without any skew between the DP159 outputs and the connector hence the layout cannot cause such large skew violation.
We have measured same values for devices with package/date codes 5c and 61.
We have also observed from the measurements (single-ended) that the negative signal output seems to be shiftet slightly lower than the positive signal. This shift will offsett the crosspoint and possibly be interpreted as a skew-fail by the compliance test setup.
With regards to these observations we have a few questions?
- How is the correlation between TMDS output pins and internal termination and/or supply pins in the device?
- Can any external signals or supplies cause a shift in the pos/neg TMDS output levels?
- Is it possible to get the compliance test report for the device?
- And is the compliance test performed on the EVM or on another implementation?
Best regards
Håvar Beyrer