Other Parts Discussed in Thread: DS90CR285, DS90CR286, DS90CR286A
hello,
in your datasheet, there is no hw schematic for connect DS90CR285 to RGB 24b interface.
thans for your support.
best regards
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: DS90CR285, DS90CR286, DS90CR286A
hello,
in your datasheet, there is no hw schematic for connect DS90CR285 to RGB 24b interface.
thans for your support.
best regards
Hi Loic,
There is no specific requirement for mapping the RGB bits to the DS90CR285 as long as they match the parallel output mapping on the deserializer side. With this having been said, the OpenLDI standard defines the typical TFT data mapping as defined in the following application note:
http://www.ti.com/lit/an/snla014/snla014.pdf
For typical mapping into the transmitter, please refer to Table 1 in the column labeled "24-bit Tx (C385)."
Thanks,
Michael
Hello,
thanks for your answer.
do you have same document about DS90CR286 please ?
thnaks
best regards
Hi Loic,
You can actually use the same application note as the one I attached in the previous thread. In the application note, to reference Rx devices like the 28-bit DS90CR286, look for the column titled 24-bit Rx (CF384A).
Thanks,
Michael
Hello Michael,
I have this interface with my LCD but it is not same maaping that is indicated in your last document.
please confirm that I need to connect for Txout0 G0 R5 R4 R3 R2 R1 R0 instead G2 R7 R6 R5 R4 R3 R2 indicated in your doc
thanks
best regrads
Hi Loic,
Thanks for the mapping. After reviewing the contents of this thread, is my understanding correct that your design does not use a DS90CR286A device at all? It seems to me that you have the following configuration:
FPGA/ASIC -> DS90CR285 -> LCD Panel
Please confirm if this is correct.
From this mapping you have provided, you will need to map "TxOUT0/RxIN0 => G0 R5 R4 R3 R2 R1 R0." This means that this LCD panel is expecting the MSBs to be located in "TxOUT3/RxIN3."
Do you have the mapping of the FPGA/ASIC outputs going into the DS90CR285 LVCMOS parallel TxIN0-27 inputs? If we know this mapping, we will be able to tell if the bits are mapped according to the positions they will appear within each LVDS data pair:
Thanks,
Michael