Other Parts Discussed in Thread: TUSB322I
The TUSB322i asks for a resistor values of 891k-909K between VBUS_DET and VBUS.
900K resistors with a 1% tolerance are hard to find.
Could i use a 909k resistor with 1% tolerance?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
It is all related to the internal VBUS threshold, and the value for the external resistor is fixed to the range 891 - 909 KOhms. You can see the values on the datasheet page 6 ( VBUS_DET IO Pin section)