I'm trying to find a easy way to use the ethernet boot loader without constantly entering in the ip and mac address each time I wanna do a version update. Is there a way just to enter in a default ip adress which all the devices have in common, enter no mac address and the bin file I need loaded. So that I can make create a batch file so it'll be a one click and go type thing instead of going through a long drawn out process each time I wanna update a device.
Please help