This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83867IR LED connection

Guru 15520 points

Other Parts Discussed in Thread: DP83867IR

Hi,

I have a question about DP83867IR LED pins which are also use as strap pins.

We are planning to connect 93637-8617(RJ45) against DP83867IR.
This RJ45 jack have two LED(pin#12 and pin#11) which are connected together inside the Jack.
(Please see the attached file page.1)

I want to connect LED_0 pin of DP83867IR to pin#12(pleas see attached file page.2)

RJ45 have two LED connected together so I wonder the route layout which I wrote in attached file are correct or not.
Are there any reccommended route layout for LED_0 pin of DP83867IR when connecting to this kind of RJ45 LED?
If there are block diagram of route layout , it is so helpful.

I checked the DP83867IR datasheet page.50 "8.5.2 LED Configuration",
but I don't understand what is the correct layout.

best regards,
g.f.

0083.DP83867IR LED pin connection.pdf

2158.936378617_sd.pdf