Other Parts Discussed in Thread: DS30BA101, DS30EA101
Dear TI Team,
We are using the Serializer (DS90UB947) & De-serializer (DS90UB948) chips for the video interface.
Both these chips are mounted on two different PCB's. A cable connects these two PCB's via the FPD-Link III.
However due to the length constraints we are getting signal integrity issues.
Request your assistance for the following two points:
1) Are there any re-drivers available for the FPD LINK-III so that the signal integrity issues can be solved.
2) What would be the maximum length/breaks possible for the FPD Link-III
Thanks.