Other Parts Discussed in Thread: DS32EL0421, DS32EL0124
Hello,
According to the datasheet:
The DS32EL0421 has a built-in DC-balance encoder to support AC-coupled applications. When enabled, the input signal on TXIN4+/- is treated as a data valid bit. If TXIN4+/- is low, then the four bit nibbles from TXIN0-TXIN3 are taken to form a 16 bit word.
My question:
I need 8b10b decoding, so I must pull TXIN4 +/- down. However, it es necessary to pull down both data lines. Is it possible to pull only one of them down and DC Balance is working?
Thank you in advance!