Other Parts Discussed in Thread: DP83620
Hi, I am using DP83620SQ/NOPB PHY for our 10/100Mbps Copper Media Ethernet Interface. We had connected through the Magnetics part "749013011A" which is not PoE supported. But we need to use this for powering external device without following the Standard PoE process (simply appending power with the data signals).
For PoE interface, the legacy (general) bob smith termination would not be suit. Hence 10nF capacitor is added along with the 75 ohm termination resistor. To increase the power handling capacity through the bob smith termination during surge condition, we are purposely added one more 10nF+75 ohm termination resistor combination along with the existing each 10nF+75 ohm termination combination.
Will this scheme affect the cable characteristic impedance matching scheme?
I had given the corresponding magnetics interface sheet for reference. Since we are closer to the LAYOUT release, expecting reply at very earliest.
Thanks,
Devendhiran