Other Parts Discussed in Thread: DS90LV001, DS10BR150, DS90LV804
I’m using nine of DS90LV001TLD-NOPB as LVDS-TO-LVDS buffers in a project . The input traces are max 1” long.
Questions:
-
Do I have to use 100-ohm termination at the input side assuming max 1” input trace length?
-
Is there an identical part (the same package) with internal termination?