This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[TPS65982] UserVIDAltModeOtherVDM Event

Customer reported that the behavior of UserVIDAltModeOtherVDM is different from firmware v1.11.04 and v1.11.05 version. Could you confirm if this is expected behavior?

 

FW v1.11.04

UserVIDAltModeOtherVDM Bit[59] of IntEvent(0x15h) is set only when Unstructured VDM is received.

 

FW v1.11.05

UserVIDAltModeOtherVDM Bit[59] of IntEvent(0x15h) is set when Discover Modes, Enter Mode and Unstructured VDM are received.

 

We provided I2C capture data on customer in separate email.

 

Considering the development schdule on customer (going to fix their EC firmware very soon), I appreciate if you give us a feedback as soon as possible.

 

Regards,

Fukui