I am using this chip in the 2 Port configuraion.
Self powered compund device with PORT1 permanently connected on same pcb (no USB power switch)
What do I have to do with the unused pins:
DM3
DP3
OVRCUR3#
OVRCUR1#
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I am using this chip in the 2 Port configuraion.
Self powered compund device with PORT1 permanently connected on same pcb (no USB power switch)
What do I have to do with the unused pins:
DM3
DP3
OVRCUR3#
OVRCUR1#
Hello Bernt,
The DP and DM signals of the unused port should be tied to ground with 15K resistors like the pull-downs used on the active ports.
Unused OVRCUR# inputs should be pulled up using a 10kOhm resistor.
Regards