This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Cannot disable DS90UB947 streaming its internal clock when no PCLK is present

Hello,

I have a problem with DS90UB947 serializer. When I stop its input PCLK clock (I cut its input signal), it still streams out some FPD Link 3 signal. The signal consists of clock of the last frequency and no data. It seems PLL has been locked to a last frequency and serializer streams out despite of lack of input (OpenLDI) PCLK signal. I have to perform serializer reset to stop streaming and restore PCLK signal to start it again. I disabled "PCLK Auto" bit in "General Configuration" register (Disable auto-switch) but with no effect.


The serializer also signalizes "PCLK Detect" bit = 1 in "General Status" register despite of PCLK clock is disconnected. I see no PCLK on oscilloscope, but this bit is still 1. It sets 1 after first valid PCLK and never goes 0 when PCLK disconnects. Is this correct behavior?

I need to stop the steaming of internal clock when PCLK is off. My device causes problems down the FPD Link. Do you know a more elegant solution than reseting the serializer every time the input PCLK stops?

Thank you.

Ondra

  • Hi Ondrej,

    did you solve the issue?

    We have an issue very similar to the yours.
    We drive the serializer DS90UB947 with a constant pixel clock at 33MHz.
    In normal cases, at receiver side (we use a DS90UB926 as deserializer) we measure the same frequency on pixel clock pin.
    When the issue occurs, at receiver side we measure a frequency of pixel clock equal to ~32.5MHz.
    In this condition all the data (R/G/B, VSYNC, HSYNC) are wrong and on video we see a flickering effect.

    By reading the internal registers of the serializer, all seem to work properly: PLL is locked and all other status bits are ok.
    To restore the full functionality a reset of the serializer must be executed.

    Thanks in advance,

    Mirko