Other Parts Discussed in Thread: DS100DF410
Dear Sir,
Q1: My customer set DF410 in SMBUS master mode and read its initial configuration from an external EEPROM when power-up, and they want to do CDR Reset operation before normal work. Whether DS100DF100 support it? if so, how to do the configuration?
Q2: On page 15 of DS100DF410, Figure 5, the address pin (A0, A1, A2) of EEPROM, it says that One or both of these lines should float for an EEPROM larger than 256 bytes. What's the reason why we need float these pin? But in the DF410EVM schematic, the EEPROM address pins are connected to GND. More detial information, on page 38 of DF410EVM document (snlu126c.pdf), RN2, RN3-EEPROM_GND_A0/1/2.
Q3: in DS100DF410 datasheet, page 16, line 10, it says that To produce the write address for the SMBus, the seven-bit address is Left-shifted by on bit. But based on the data in table 2, it seems that Right-shifted, not Left-shifted. Can you confirm it?
Q4: Can you send me a timing wave of DF410 reading in SMBus master mode when power-up for reference, based on DS100DF410EVM?
Thanks a lot!
Regards,
Jack