Other Parts Discussed in Thread: DS90CF384A
Hi Team,
The customer wants to use DS90CF384A. From data sheet it is clear that DS90CF384A is gives parallel 28 bits of CMOS/TTL data.
But In the customer's application he needs an option to use only three LVDS data receiver channels to get 21 bits of CMOS/TTL data. In datasheet, there is no evidence regarding this.
Q1: Can you please let me know if this kind of usage is correct. If this usage is correct, which pins are the output pins when the input pin is RXIN0?
Which pins are the output pins when the input pin is RXIN1?
Which pins are the output pins when the input pin is RXIN2?
Which pins are the output pins when the input pin is RXIN3?
Q2: If this usage is correct, how to deal with all un-used pins? Should be pulled down all un-used pins?
Thanks,
Best Regard