This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Build error on WDK7600



Hello,

I'm very sorry for coming back to the same question.
I made some misunderstanding.

In fact...

1) I merged co-installer source code and TUSBWINVCP source code.
   And I built on WDK7600 supported Windows7, error occurred.

2) When I used WDK7600 not supported Windows7, error did not occur.

I would like to know the right combination of each source code version. 

And I ask again the following question.

The reason why I compile this time is that I want to change the file name of installer. 
I am afraid that some problems occur when I connect two different USB devices to the same PC.
These USB devices have different drivers and the same installer file name.
If I use the default file name for USB device, it is possible to conflict to the same file name, I think.
Am I right?


Best Regards,

KAZU