This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Question about TPS65982 and HD3SS460 design

Guru 19685 points

Other Parts Discussed in Thread: HD3SS460, TPS65982

Please let me know about four points below of TPS65982 and HD3SS460 design.

-----------------------------------------------------

①Are signal inputs (USB,DP,AUX) need to connect input capacitor?

②TPS65982: PP_5V0 's source power rail need to use current limit or system power input, is it correct?

③From CPU, is DP AUX signal need to connect TPS65982 or HD3SS460?

④Are TPS65982 and HD3SS460 's supply voltage need to the same power line?

-----------------------------------------------------

Best regards,

Satoshi