Other Parts Discussed in Thread: DS90C031
Single ended signal to LVDS:
When I input 80Mhz clock 50-50 duty cycle. LVDS output has a Duty cycle of approximately 55-45. is this normal behavior?
/B
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: DS90C031
Single ended signal to LVDS:
When I input 80Mhz clock 50-50 duty cycle. LVDS output has a Duty cycle of approximately 55-45. is this normal behavior?
/B
Hi Bob,
Is your input signal 0 - 5V or 0 - 3V? The input threshold for the DS90C031 is ~ 1.5V. If a 0 - 5V signal is used, it will tend to cause some duty cycle distortion as the frequency increases.
Regards,
Lee