Other Parts Discussed in Thread: TPS65982, TPS65982-EVM
Hi,
I'd like to know the recommended power supply for PPCABLE in the TPS65982.
The datasheet mentions IPPCABLELIMIT (lowest and highest). Let's say 600 mA max.
That means that I have to design my voltage regulator to 5V/1A. Is this really so ? Or is there a min. current consumption at which is it ok ?
Then I can take another regulator.
Other question : Must I necessarily use the same supply for PPCABLE and PP_5V ?
Thanks in advance and for the good job.
YG.