Other Parts Discussed in Thread: TCA9548A
are starting to look for parts for a new project and I need an I2C bus MUX
The CPU I use is at 1.8V levels
The devices I use are at 3.3V levels
found the part TCA9548A that claims support level translation
The problem is I don’t see this from the data sheet as the VIH and the VOH will not work in mixed level system
- Can you please look if this is correct?Am I missing something?
- Can you recommend a different part that will do this
- Can I use an external level transition parts that will work with this part?