Other Parts Discussed in Thread: LMP7701
[ LMH1982 ] No lock indication of SD_LOCK
Hi,
Can you help to clarify the behavior which SD_LOCK does not indicate lock status as expected.
My customer has reported following information.
* SD_LOCK is NOT asserted.
* However It seems that the input reference and output clock are in-lock. (checked by oscilloscope.)
(It seems that device is not in FREE RUN mode.)
I have checked some points from customer circuit and register settings as below.
- LOCK_CTRL: max (0x01h = F8h)
- REF_VALID, HD_LOCK are asserted.
- Customer changes REF_DIV, FB_DIV and ICP1 based on input format.
- ICP1 setting is enough large compare with limitation (described in datasheet)
- no High-Z amp (ex LMP7701) is used in loop filter circuit.
I'm bit concerned that they don't have high-z amp, so the leakage current would prevent device to establish valid lock condition. So may be it's reasonable to check the behavior with slightly larger ICP1 value.
It's really appreciated, if you have any comments and/or ideas.
Thank you for your support in advance.
Regards,
Ken