Other Parts Discussed in Thread: TUSB1211
Hello, I'm looking at the feasibility of a design where I use the MCU with your USB HS PHY: TUSB1211 to act as a USB HS host. I need it to be in a sleep, standby, or other low power mode such that the current consumption from my board is less than 1mA. Ideally, I would supply the MCU with just VBAT at this point. I then need it to sense when a USB device is plugged into it, then it will wake up once a device is plugged in. Does the USB peripheral support this type of operation with the low current performance? Does your PHY support this or any other PHY you can suggest? Do you have any solution to this? Thank you. Nicolas.]