Other Parts Discussed in Thread: SN65LVDS93A
Hi guys,
We are using a SN65LVDS93A to serialise camera data for a FPGA. During power-up of the FPGA, we found that the FPGA is driving 1.8V through internal 25kOhm resistors to the SN65LVDS93A outputs. These 1.8V are present for ca. 7 seconds until the FPGA is fully configured. During this phase, the SN65LVDS93A is still unpowered.
According the datasheet, no voltages greater than Vcc+0.5V are allowed at the outputs, which would be in our case 0.5V. But before we spend some extra circuitry to protect the SN65LVDS93A outputs, we would like to know if these 1.8V pulled through a 25kOhm resistors are really an issue? Because 1) current into pins is very low and 2) other TI serializers with LVDS output have a similar output circuit but maximum output voltage is not Vcc referenced.
Thanks,
Patrick