Other Parts Discussed in Thread: SN65DSI86
Hi,everybody.
My sn65dsi86 work well on color bar mode,and the mipi driver also work well on a mipi LCD panel. I have two questions need you help.
1、
Now I use sn65dsi86 instead of the mipi LCD panel ,convert MIPI to EDP signal.
I have been changed h-active,v-active,hbp,hfb,hpw,vbp,vfb,vpw parameter as same as the parameters of sn65dsi86,and the parameters is work well on color bar mode. But the edp lcd is back,just seeing backlight. why? Must i change the MIPI driver code to adjust the sn65dis86 chip? If need to change the code ,please give me some example,thanks.
2、What is the most largest pixel when just using single CHA 0f sn65dsi86 ?my edp LCD is IPAD mini2 ,the pixcel is 2048*1536. should I use single CHA or CHA and CHB?