Hi all
Would you mind if we ask DP83867IR?
Our customer would like to use the attachment file's RJ45 with pulse trans.
20160923_RJ45 connector with PulseTrans.pdf
<Question>
We have heard followings on Ether-forum;
-Center tap is pulled to VDD since the driver we use is a current mode driver.
-If it were a voltage mode driver we would have center tap to GND.
-Since the transformer isolated the ground planes between the link partners, we can use either type.
Is DP83867IR the current mode driver or the voltage mode?
How much of Pull-up voltage is suitable? VDDIO level?
Kind regards,
Hirotaka Matsumoto