Other Parts Discussed in Thread: TUSB7320, TUSB7340
Hi,
I have two questions on TUSB7320 device, they are
1. In TUSB7320 device, 1.8V supply is being to clock the oscillator. Can the clock oscillator be enabled before the VDD33 and VDD11 supplies come up? Or it need to be enabled after VDD33 and VDD11 supplies have ramped up.
2. PERST# in my design is being controlled by a GPIO of PCIe host. During Power Down sequence, the PERST# signal will get asserted and the PCIE REFCLK clocks will get disabled simultaneously. Then after a few ms the VDD33 and VDD11 will be removed. Is this fine?
3. Does the TUSB7320 device require ac coupling and 100 ohms parallel termination to interface with a HCSL clock driver output?
Thanks,
Shareef