Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Questions about TPS65983 Configuration tool v2.10

I have some question about v2.10 configuration tool (64 bits).

1. The default project template of Bus-powered device is removed, then which template I should use if our device is Bus-powered device in Tool v2.10?

Tool v2.9

Tool v2.10

2. The new metadata “XID”, should I leave it as default or customize it to PCI vendor ID, Thunderbolt device ID or something else?

3. When I save the project configuration, the shared device settings tab splits to two tabs(Device 1 and Device 2), is it correct?

If I load the saved project file, the split two tabs merge to one shared device setting tab again, even the “Share Settings Across All Channels” box always checked. What I am concerned about is the Number of Connected Devices setting is 1 or 2 if I use this project setting?

 

Step 1. fill out the form, there is only one device setting tab.

 

Step 2. Save the project configuration

 

Step 3. After the project is saved, the device setting tab splits to two device tabs

 

Step 4. Load the saved project file again

 

Step 5. Two device tabs merge to one device tab

 

I look forward to receiving your reply soon.

 

Regards,

Axel