Other Parts Discussed in Thread: TFP410
Hi,
I am looking for a 18 bpp Digital RGB to HDMI Transmitter chip .Plz. suggest any part no. for the same.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: TFP410
Hi,
I am looking for a 18 bpp Digital RGB to HDMI Transmitter chip .Plz. suggest any part no. for the same.
Hi Abhishek,
The only HDMI serializer we have is TFP410, take a look at it and determine if it meet your needs.
Regards
Hi,
Thanks for ur reply.
But here I am looking for a chip which takes 24 bit digital RGB as input and converts it to HDMI output. That is Digital RGB to HDMI converter.
please help me for the same.
Hi Abhishek,
TFP410 works as RGB to HDMI converter, with the limitation that it only transmits video, audio would have to be transmitted out of HMDI link.
This is the only device we have for RGB to DVI/HDMI cnnversion.
Regards
Thanks for your reply.
Can u confirm whether DVI ports can be used as Digital RGB (24-bit) with input signals such as:
VPA[0:5] ,VPB[0:5],VPC[0:5],Hsync,Vsync,DE,CLK.
Please comment.
please clarify wrt TFP410 chip:
1- RGB666 format i.e RGB x 6 bit each (18 bpp mode) input can be fed to the input bus Data[23:0] of TFp410.
Hi Abhishek,
Yes you cna use 6 bits per color, you have to use the most significant bits of each color and connect the two least significant bits to GND.
TFP410 will transmit 8 bits per color over the HDMI link.
Regards
Thank you so much for clarifications.
Plz. let me know:
1- Any application notes or reference design for the TFP410 with similar application or any.
2- timing diagram for 8 bits per colour mode.
2- Chip life time and lead time.
3- Can I get any samples of TFP410.
Looking for your further support.