Other Parts Discussed in Thread: SN65DP159
Hello...
We use SN65DP159 in redriver mode... and the device often dies, which means one of TMDS Output Channel does not working..
I connected TMDS output directly to the HDMI Connector with no termination and 3.3V Termination is on the Receiver Side.. and do not use auto power down.
My guess is
(1) SN65DP159 is damaged when HDMI Cable Connects on and off.. (since there is no ESD protection diode)
(2) if one of TX and RX Board is not powered on, the chip is damaged by current injection.
(3) TMDS Output driving with no termination may damage the chip. (when cable is not connected..)
I wonder what is the main reason of the chip damage.. Is there any experience about this ?
What is the correct connection of the chip to be protected safely?
One more question is as below :
According to the datasheet, input signal is terminated on Vbias inside chip and it looks like 0.7V... but when I monitored with oscilloscope, VCM of input signal is almost 0V. Is that right?? I thought it would be higher then 0V, some level between 0V and 0.7V.. (input signal is ac-coupled.)