Hi,
I am new to here, so If I post question in wrong place, please let me know and sorry about that.
I have a Ti processor AM335x on a dev board. right not there are two uart connect to processor. uart0 and uart2
by default, only uart0 was enable, and it was for console. after I enable uart2, I wired my GPS to it so that it should output something if I cat /dev/ttyO2. but there are only some garbage code shows up.
then I wired GPS to uart0, use same command cat /dev/ttyO0 everything works fine. GPS output shows up normally.
then I edit my uEnv.txt to switch my console to uart2, it works. and then I wired GPS to uart2, I can cat /dev/ttyO2 to get everything. But when I wired GPS to uart0. garbage code shows up.
I did use stty to do tty setup, make them all same, still, I can only read from the uart which I connect my console.
I run command dmesg | grep tty , this is the output
[0.000000] Kernel command line: console=ttyO2,115200n8 root=/dev/mmcblk0 rw ext4 rootwait verbose debug
[0.234749] 44e09000.serial: ttyO0 at MMIO 0x44e09000 (irq = 154m, base_baud = 3000000) is a OMAP UART0
[0.235338] 48024000.serial: ttyO2 at MMIO 0x48024000 (irq = 155m, base_baud = 3000000) is a OMAP UART2
[0.824084] console [ttyO2] enabled
first and fourth would change base on which uart I put my console on.
Are there any config I missed? why I can only read precise data from the uart I put my console on. and others doesn't work.
any idea would help. Thanks.