Dear, All
The customer wants to connect I.MX6 of NXP and SN65DSI86.
They want to be connected in MIPI I/F.
However, I.MX6 is following I/F.
- DSI Version: 1.01
- MIPI D-PHY Vorsion: 1.0
- The number of DSI Lane: 2
SN65DSI86 is following I/F.
- DSI Version: 1.02
- MIPI D-PHY Vorsion: 1.1
- The number of DSI Lane: Max 4
When we connected these, does this work without a problem?
Thanks, Masami M.