Other Parts Discussed in Thread: DS250DF810
Hello,
After following the EVM setup guide for both sigcon architect and the ds250df810 evm I'm still stuck by the device not being recognized on any of the slave addresses. I get the "Invalid Address or Device Not Active" error. It should be 0x30 according to the user's guide (I verified all jumpers according to the image shown). I did install the sigcon architect add-on for the DF810. The EVM is powered on 3.3 V, connected over USB.
Any ideas?
Thanks,
Michael