Other Parts Discussed in Thread: SN75DP139
Dears
I have a customer using SN75DP139 between Intel CPU and a DVI connector, and find some failure. one of the output channel have lower signal amplitude is the phenomenon. and we also checked the DC level of the signal, and the failure channel have like 1.6V DC offset, but the normal channel have 2.9V offset.
we also try to add 50Ω terminal resistance on the output, but the DC level is still 1.6V, seemed the IC draw lots of current.
so is there some suggestion in your side about this failure? customer do not add the 50Ω input terminal resistor, does this have impact.
and also they do not connect the I2C pin, is it OK?
Thanks
Jun Shen