Other Parts Discussed in Thread: TPS65982, TPS65982-EVM
Hi,
I just fell over one point within the TPS65982 Application Customization Tool: I started to configure the GPIOs but I can "only" see GPIO 0 / 1 / 2 / 3 / 6 / 7 / 8 / 12..16. So, there is no means to configure GPIO 4 / 5 / 9 / 10 / 11.
At the moment I'm working on the TPS65982-EVM, and according to the schematics of the EVM and the datasheet of the chip those GPIOs are present; and used (in case of the EVM; e.g GPIO 5 is used as in Input).
Am I missing something or are these GPIOs excluded on purpose?
Thank you for any help and hint,
kind regards,
Georg