Is it possible to use the DEN signal to the DS92LV1021 or SN65LV1023A to send a single data ‘frame’ of 10 bits? Assuming that one can’t simply stop and start TCLK on a whim in order for the PLL to remain running, then can one strobe DEN in order to send a single ‘frame’ intermittently rather than an infinite stream of frames?
The timing diagram in the datasheet only show the relationship between DEN and Dout+/-, but not that of DEN to the data frame. If DEN is not synchronized to the frame start internally, then the frame would presumably be truncated somewhere in the middle of the transmission.
Regards,
Steve