Other Parts Discussed in Thread: DAC8750
Hi, As you know IO-Link technology is used in switch/ sensor where analog output is also required so is it possible to have analog output on the same transceiver chip?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: DAC8750
Hi, As you know IO-Link technology is used in switch/ sensor where analog output is also required so is it possible to have analog output on the same transceiver chip?
Hi Max,
Thanks for your answer.
You are right IO-Link specification does not talk about analog outputs on connector pins. But most of the switches/ sensors available in market are provided with analog output on the other pin like this,
So to provide this analog output we need to have separate DAC IC (may be TI - DAC8750) or MCU with in built DAC and some discrete components.
If we've a single chip solution with switching output OR IO-Link(this is already there in SN65HVD10x) and one more switching output OR 4-20mA analog output, then it will be best option to design such kind of sensor with minimum components because these sensors are small in size so PCB size should be small. As of now there is no such IC available in market but if it is available then it will be easy for development.
Hi,
What are the thoughts of your team regarding single chip solution.
One more thing Can we develop Micro controller to IO-Link level signal without transceiver? Is it possible to design this transceiver using discrete components?
Thanks,