Hello,
How do you know which pin is pin 1 on the chip tpd1e05u06 (package 2-Pin X1SON) ?
For the two other packages (10-pin and 14-pin) it is clearly marked with a point on pin 1.
What about 2-pin chip?
Thanks in advance,
Hermine
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
How do you know which pin is pin 1 on the chip tpd1e05u06 (package 2-Pin X1SON) ?
For the two other packages (10-pin and 14-pin) it is clearly marked with a point on pin 1.
What about 2-pin chip?
Thanks in advance,
Hermine
Geoff-
Thanks for keeping track! The most recent datasheet update was to correct a different minor issue in the datasheet; the pin polarity marking should be added within the next week or so. Until then however, just know that pin 1 on the IC is designated by a line printed on the top!
Thanks,
Alec
Hello,
There is a line on the package itself that should be above the the letters on the device. Also the marking for the TPD1E05U06 is not PB, it should be C1, C2, C6 as said on addendum page 1 of the datasheet. Are you sure that the device you are inspecting is the TPD1E05U06?
Regards,
Cameron