The datasheet describes the default polarity of LED_0, 1 and 2 in part of "LED Configuration Resister2". The default is active high.
When user set mode4 for the LED pins as the strap function, is the default polarity automatically changed to active low? Or user have to change the register bit value of LED_x_POLARITY?
Best Regards