Other Parts Discussed in Thread: TLK2501
My customer is asking the following questions:
I am not having any issues with the TLK2501, but that I am suspecting the board layout leading up to the TLK2501 as the root cause of the poor impedance I am seeing when looking into pin 53 (and 54).
I am an RF circuit designer by background and my tool of choice for looking into issues like this is with a network analyzer. For the particular board of concern we have two SMA connectors which lead to the serial receive inputs, DINRXP and DINRXN. When I hook up the network analyzer I see a very poor return loss, particularly at our chosen data rate.
I would like to find out a couple of things:
Do you have any network analyzer s11 measured results from that board which can be shared? I assume the EVM is layed out well and I would like to see how good that impedance can look.
From the datasheet the input capacitance for the TLK2501 has a max value of 2pF. Do you have a typical value or any more detailed information I could use for a circuit model? I typically use Agilent’s ADS RF simulator for circuit analysis and don’t typically work with IBIS models.
Can we help them either with S11 data or with more detailed information in the input capacitance of the part?
Thanks for your help with this!
Richard Elmquist