This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Driver questions about DP83867



Does DP83867 support reference code with OS Windows Embedded Compact 7?

Does DP83867 need special driver supporting in conventional Windows and Linux OS? 

  • Hi Peter,

    We do not have sample code for Windows Embedded Compact 7.

    The DP83867 does have driver support for Linux OS but it is not required to be used. The generic Enet PHY driver can be used for Linux. I suspect the same for Windows, but there may be OS side dependencies I am not familiar with. From the perspective of the DP83867, all options for typical use can be set using the strap pins.

    Best Regards,