Other Parts Discussed in Thread: DP83848I
Hi Team,
The customer is using DP83848I .
Q1: What is the function for the address pins(COL, RXD1_0,RXD1_1,RXD1_2, and RXD1_3)? When the customer can use the address pins?
Q2: The customer has done two HUBs in FPGA and he needs to connect two PHYs. Can the address pins be used? If the address pins are connected, how to
connected? Please send me the reference schematic for DP83848I.
Thanks,
Best Regards,